External Upconverter

For M9484C with Option AL2. 

Type of Supported Upconverters

LO1 and LO2 Connectors For Use With V3080A

RF Channels Connectivity For V3080A

Integrated Operation with an Upconverter

Automatic Upconverter Detection on Startup

GUI and SCPI Settings to Configure an Upconverter

Upconverter Model

Upconverter Serial Number

IF Cable File

Custom IF Cable File

Type of Supported Upconverters

You can use the following external upconverter models with your signal generator.

Upconverter Model Upconverter Type Required LO
Keysight Technologies V3080A Controlled Auxiliary LO @ 9.6 GHz

All upconverters utilize the RF and appropriate LO outputs from the source for the IF and LO inputs of the upconverter, respectively.

The V3080A upconverter requires the use of the Auxiliary LO operating at 9.6 GHz. This LO is present on M9484C with Option AL2.

LO1 and LO2 Connectors For Use With V3080A

The instrument contains two connectors labeled LO1 and LO2 for providing an Auxiliary Local Oscillator output. Each connector can be off, or provide a CW frequency of 2.4 GHz, 4.8 GHz, 9.6 GHz, or 19.2 GHz. If you are not using the output, place the setting to off to minimize emissions.

When using the V3080A Frequency Extender, the Auxiliary LO connector(s) are used for interfacing with V3080A. With a V3080A connected, the auxiliary LO port is set to 9.6 GHz and is not changeable.

When one V3080A is connected to the instrument, the LO1 will be used. If a second V3080A is connected, LO2 will be used.

RF Channels Connectivity For V3080A

You can connect one or two V3080As to a 2-Channel M9484C VXG.

If you want to connect a single V3080A to a 2-Channel M9484C, then you must connect it to Channel 1 of M9484C.

On M9484C, the upconverter must be connected at start-up. Once connected at start-up, it will remain enabled.

Integrated Operation with an Upconverter

When an upconverter is enabled (in use), it is integrated into the operation of a channel in the following ways:

Automatic Upconverter Detection on Startup

On start-up, an instrument automatically detects if a supported, controlled upconverter is connected, and attempts to enable it. This process performs LO and IF power checks (as well as communication checks) to determine if the upconverter is fully connected and operational. If this check succeeds, the upconverter is enabled on the connected channel, otherwise errors are shown in the Message queue.

For M9484C, in the event of errors, the instrument needs to be powered down to resolve the issue and then powered up to attempt to enable the upconverter. All external upconverter configuration settings are accessible via the Configure Launch option in the System Menu.

GUI and SCPI Settings to Configure an Upconverter

Upconverter Model

The model of the upconverter to be used on the specified channel. Supported upconverter options:

SCPI Command

:ROUTe:EUConverter<channel>:MODel NONE|K80A

:ROUTe:EUConverter<channel>:MODel?

SCPI Example

ROUT:EUC1:MOD K80A

ROUT:EUC1:MOD?

Notes

For M9484C:

With or without option AL2, the upconverter model can only be queried. When no upconverter is connected, NONE is returned, otherwise K80A is returned, for the supported model V3080A. Attempting to change upconverter model raises the error "Feature not supported; Setting upconverter model unavailable on this instrument."

Dependencies Upconverter Model can only be changed if the upconverter is not enabled.
Preset This is unaffected by a Preset but is set to NONE on a "Restore System Settings to Default Values."
Range None|V3080A
State Saved Persistent, survives preset and power cycle but not saved in the instrument state.
Initial S/W Revision A.18.00

Upconverter Serial Number

Query only.

Returns the serial number of the upconverter, when a Keysight Technologies upconverter is enabled.

SCPI Command

:ROUTe:EUConverter<channel>:SNUMber?

SCPI Example

ROUT:EUC:SNUM?

Notes If no Keysight upconverter is enabled, returns "".
Preset ""
State Saved No
Initial S/W Revision A.18.00

IF Cable File

The characteristics of the cable used to provide the IF signal to the upconverter can be specified to improve the IF power accuracy into the upconverter.

If you are using the 1 Meter, 2 Meter, or 3 Meter cable purchased from Keysight Technologies, the .s2p characteristics are included in the instrument's software.

If you are using a cable obtained elsewhere, select Custom and provide the path to the .s2p file in the Custom IF Cable File setting.

The IF Cable loss data affects the IF power into and the RF power out of the upconverter.

If the data in the selected file does not match the characteristics of the utilized cable, inaccurate corrections will be applied.
SCPI Command

:ROUTe:EUConverter<channel>:IFCable IDEal|C_1M|C_2M|C_3M|CUSTom

:ROUTe:EUConverter<channel>:IFCable?

SCPI Example

ROUT:EUC:IFC C_3M

ROUT:EUC:IFC?

Notes

For M9484C without Option AL2:

Attempting to change EUC raises error 703,"Feature not supported; IF Cable unavailable, AL2 is required."

Selecting IDEal results in using 0 dB for the cable loss.

For the V3080A:

C_1M|C_2M|C_3M|IDEal|CUSTom can be selected.
When a V3080A model is selected and the IF Cable will be updated to C_2M.
If a V3080A is detected and enabled on start-up and IF Cable is IDEal, it will be updated to C_2M.

For all other upconverters:
Only IDEal|CUSTom can be selected.
Changing the upconverter model will update this to IDEal (except as noted above).
Changing the IF Cable can affect the IF power into and RF power out of the upconverter.
Preset

For M9484C:

C_2M

This is unaffected by a Preset but is set to default value on a "Restore System Settings to Default Values."

Range Ideal|Cable_1M.s2p|Cable_2M.s2p|Cable_3M.s2p|Custom File
State Saved Persistent, survives preset and power cycle but not saved in the instrument state.
Initial S/W Revision A.11.00
Modified at S/W Revision A.18.00 - Added IDEal option

Custom IF Cable File

The .s2p file for the custom IF cable must be uploaded to the instrument prior to specifying the cable for use via the following command (as a CUSTom cable).

Custom Cable Files should be stored in the ExternalUpconverter directory of the Corrections Folder.

The following table shows few custom cable file path examples and which folders are selected.

SCPI command example Folder
ROUT:EUC:IFC:CUST "abc.s2p" <Documents>\Keysight\PathWave\SignalGenerator\Corrections\ExternalUpconverter
ROUT:EUC:IFC:CUST "myDir\abc.s2p" <Documents>\Keysight\PathWave\SignalGenerator\Corrections\ExternalUpconverter\myDir
ROUT:EUC:IFC:CUST "C:\wfm\abc.s2p" C:\wfm\
Only .s2p file types are accepted and custom IF and LO cable filenames should be distinct.
SCPI Command

:ROUTe:EUConverter<channel>:IFCable:CUSTom "<path>\<file_name>.s2p"

:ROUTe:EUConverter<channel>:IFCable:CUSTom?

SCPI Example

ROUT:EUC:IFC:CUST "<Documents>\Keysight\PathWave\SignalGenerator\Corrections\ExternalUpconverter\custom_cable_file.s2p"

ROUT:EUC:IFC:CUST?

Notes For M9484C without option AL2:
Attempting to change raises error 703,"Feature not supported; Custom IF Cable File unavailable, AL2 is required."
Attempting to change to a filetype that is not .s2p raises error 629, "File format invalid:Invalid Custom IF Cable File selected."
Dependencies Applies only when Upconverter IF Cable File is CUSTom.
Preset This is unaffected by a Preset but is set to an empty string on a "Restore System Settings to Default Values."
State Saved Persistent, survives preset and power cycle but not saved in the instrument state.
Initial S/W Revision A.11.00